This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps54821参数

Other Parts Discussed in Thread: TPS54821

用tps54821输出1.03V,要求如下:

Output Voltage 1.03 V

Output Current 8 A

ΔVout = 5 %

Input Voltage 12 V

Output Voltage Ripple 30 mV p-p

Switching Frequency 480 kHz

能否告诉我电感,输出电容,和补偿电阻电容的参数。