This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps65217c锂电池接入会一直供电,如何才能硬件或软件控制变为off或sleep状态?



Hi ,大家好:

现在基于类似于BBB的开发板,使用的电源管理芯片是TPS65217C,我想外接DC断电时内置3.7V锂电池工作继续供电。现在的问题是,外接电源断开,锂电池供电这个很正常,锂电池处于供电状态时,我想通过软件或硬件来控制芯片变为OFF 或SLLEP,可是不能实现。

1.首先我想通过拉低PB_IN 大于8s时间,发现开发板会不断重启,而不是sleep。当只有外部电源供电时(内置锂电池没有接),正常状态下拉低PB_IN会正常关机,这个是什么原因?

2.尝试拉低PB_IN不行,我想通过halt 或poweroff来关机,发现现象还是重启设备,不能正常关机。

  • 1. 你检测下你的系统应该是进入如下这种情况了,因此再同时比较下你现在测试的两种情况下nRESET脚的电平情况,这块可能会有些影响

         If the PB_IN pin is kept low for an extended amount of time, the device will continue to cycle between ACTIVE and RESET state, entering RESET every 8 s.

    2. 要实现关机,如下方法都可以的啊!

         A power-down sequence is executed if one of the following events occurs:

    • The SEQDWN bit is set.
    • The PWR_EN pin is pulled low.
    • The push-button is pressed for > 8 s.
    • The nRESET pin is pulled low.
    • A fault occurs in the IC (OTS, UVLO, PGOOD failure).
    • The PWR_EN pin is not asserted (pulled high) within 5 seconds of a power-up event and the OFF bit is set to 1.