我的电源输入端接的是7节串联的4.2v锂电池,相当于29.4v,我需要同时给输出12v,5v,另外我的锂电池需要给drv8711供电驱动步进电机,我希望用LM2588设计2路不共地隔离12v、5v,但是我看参考设计里面vin小于30v,我能用LM2588设计吗
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
虽然LM2588的耐压值可以到40v,但LM2588的工作电压范围和变压器砸比和输出电压大小有.采用反激的多绕组变压器可以实现5v和12v隔离输出,无需两片IC。
如果12v@1A再加上5v功率,LM2588可能会有点问题.可以考虑LM3481, MOSFET外挂方案.实现原理一样,都是采用反激拓扑结构,不过需要自己设计变压器。
Hi:
上述方案见网站:
http://www.ti.com.cn/product/cn/LM2587/technicaldocuments
中的方案:AN-1095 Design of Isolated Converters Using Simple Switchers
http://www.ti.com.cn/cn/lit/an/snva005b/snva005b.pdf
Hi
做反激输入电压不宜过高,要留有裕量。
按照datasheet上,输入超过12V就有加snubber电路。