This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问BQ24040如何进入TTDM模式

Other Parts Discussed in Thread: BQ24040

TI工程师:

        我在查阅BQ24040 datasheet时,发现了有关TTDM模式的以下描述:

        (1)The TS terminal has two additional features, when the TS terminal is pulled low or floated/driven high. A low disables charge (similar to a high on the BAT_EN feature) and a high puts the charger in TTDM.

        (2)If NTC sensing is not needed, connect this terminal to VSS through an external 10 kΩ resistor. A 250kΩ from TS to ground will prevent IC entering TTDM mode when battery with thermistor is removed.

        如上所述,我使用TS脚10K下拉到地,是否是进入了TTDM模式呢?

        多谢指点。