手上有LM2675,原先是用一个24V恒压源,用LM2675转换成7V,再换成5V、3.3V给电路供电,然后控制一个6W的LED进行光通信。
现在是换了一个大功率48W的照明LED,其自带的电源是27~36V,1.25A的恒流源。考虑效率与LED寿命,LED驱动还是用恒流源好。
请问能直接用这个恒流电源给原电路供电吗?
LM2675手册上最大是输入是40V,但是没有最大输入电流?1.25A它能受得了吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Jeff,你好!
我的电路直接用5V供电电流是200mA,也就是说功率1W,1W / 36V = 0.028A,1.25A - 0.028A = 1.22A。
也就是说输出到LED上的电流还有1.22A,请问这样算对吗? 谢谢!