This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看了数据手册 里面只有输出5V的例程图 如何才能输出12V的电压
Hi,
DS中只有5v的参考电路,可以采用TI官网的WEBENCH来进行你的电路设计,如下链接,输入VIN,Vout和Iout 即可.
http://www.ti.com/sitesearch/docs/universalsearch.tsp?searchTerm=LM2621#linkId=1&src=top
在这里面输入 然后进行设计 出来的是推荐芯片 并不是LM2621输出12V的电路图 该怎么办?
你输入你的参数就可以的,输入电压会到14V?
不行啊 我输入我要的参数 都在其范围内 但是就是不行