This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于bq34z100-g1 负载模式的疑问

Other Parts Discussed in Thread: BQ34Z100-G1

1、bq34z100-g1 datasheet 8.3.6.1和8.3.6.2中说,恒流负载和恒功率负载二选一。但是在实际使用中,机器处于待机状态时,负载电流可能是1A,机器正常工作时,负载电流可能是3A、4A或5A,既不是恒流也不属于恒功率,在这种情况下,Load Mode和Load Select如何设置呢?

2、电池从满状态开始放电到放完电,这一过程中,Cycle Count的值从0变到了5,现在在充电,又变成了10,而不是从0到1再到2,是什么原因呢?

以上2个问题,谢谢帮助。

  • 1. 定电流和定功率的计算方式不一样,你可以选择定功率

    2. cycle count的值变异常,可以看一下 CC Threshold值设定是否有问题。

    One cycle occurs when accumulated discharge ≥ CC Threshold