This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教:BQ76940的电池自平衡功能

Other Parts Discussed in Thread: BQ76940

Multiple cells may be simultaneously balanced. It is left to the user’s discretion to determine the ideal
number of cells to concurrently balance. Adjacent cells should not be balanced simultaneously. This may
cause cell pins to exceed their absolute maximum conditions and is also not recommended for external
balancing implementations. Additionally, if internal balancing is used, care should be taken to avoid
exceeding package power dissipation ratings.


The host controller must ensure that no two adjacent cells are balanced simultaneously
within each set of the following:
• VC1–VC5
• VC6–VC10
• VC11–VC15

我看了BQ76940的规格书,其中关于电池自平衡部分有上面这段描述。高亮部分不明白,相邻的电池不能同时启用自平衡功能?

后面说的电池分成三组,我在猜想是不是意思就是说,相邻的电池组不能同时启用自平衡功能,而不是相邻的单节电池。