This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq24725A 如何实现恒流充和恒压充

Other Parts Discussed in Thread: BQ24725

我现在的充电控制是这样设置的,0x14(charge current)设置为2560mA,0x15(charge voltage)设置为1680mV,0x3F(input current)设置为2688mA,0x12(charge option )设置为0xF902,开始充电后,定期喂狗。电池为4串,满电电压为16.8v,有电量检测芯片,充电过程中定期读取电池电量,电量为100%后停止充电。我想问的是,在整个充电过程中,是恒压充的还是恒流充的(在喂狗时,我就是把充电电流重新写了一下,值还是开始设置的2560mA).

电池手册上写的充电方法为:先0.5c恒流充值16.8V,然后在恒压充电,直至充电电流<0.01c后停止充电。请问如何用bq24725实现这个充电过程?