This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116 負載的問題~

Other Parts Discussed in Thread: LM5116

您好~

我利用LM5116設計一片DC-to-DC,輸入電壓是 44~48VDC,輸出電壓是 12VDC,希望的輸出電流最大為8A,我是利用10歐姆300W的電阻來當作負載。線路設計主要是採用WEBENCH建議的線路,各項RC的數值則是參考AN-1713 LM5116-12 EVM Board (會不採用WEBENCH線路的RC值是因為先前套用過,但一上負載,就出問題(SW波形會抖,抖一抖就無輸出了))。 代理商FAE建議我採用LM5116-12 EVM Board 的各項 RC值試試(電感12uH 用的是Bourns PM2110-120K-RC)。

目前SW的頻率設定是250KHz,在調整電阻使其輸出電流為3A左右,一切正常。(有沒有加負載,SW的波形都沒有變動)可是當負載電阻設定為2.2歐姆時,照理說應該要有5A以上的電流輸出,但實際量測電流卻只有4A多(這是第一個奇怪的點)。沒經幾分鐘後就無電流輸出了,雖然SW的波形還是正常的,電壓量測也是12V。不知道是不是進入DATA Sheet 第14頁中寫的"UVLO電壓過低(忘記量測)致使LM5116進入Standby模式"?

為釐清是否為個案,所以我另外又做了一片板子來測試。測試過程與先前一致,結果也是一樣,電流上4A沒多久就無電流輸出(此時SW波形與電壓皆與有輸出時一樣)。靜置一段時間重新上電後則又恢復有電流輸出。

請問這可能是哪裡的問題呢? 謝謝您了~ 

 

 

DC-DC, 20160726.pdf
  • Hi,

       加2.2欧姆电阻时,测试电流为4A多,那么此时的输出电压已经掉了,电路出现过载.

       但是没过几分钟没有电流输出了,但输出电压是12v,这有点矛盾.如果有输出12v,带的是电阻负载,为什么没有电流呢 ?I=Vout/R。。。。

       1. 重点给看看过流点的设定是否合理;

       2. 电流检测电阻的采样电路走线是否按照差分走线;