封装必须是SOT-23-3
耐压:15V或以上
要求低功耗
输出电压3V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们的产品是用1~4节锂电池串联或者并联供电的便携式产品,用这个LDO给单片机供电的,工作电流不大,50mA以下。之前用的是MCP1703T-3002E/CB,但是由于微芯公司年后收购了两家公司,供货周期变长了,导致我们多款使用了这个芯片的产品生产受到影响。想找一个引脚和封装都兼容的芯片代替,参数也要差不多才行。要求待机功耗在10uA以下,工作温度能达到125°C是最好的,不行的话,85°C可以。
输出一定要是3V的,因为锂电池在3~3.3V的时候还是有电的,如果用3.3V的LDO,锂电池电压3.3V以下就无法稳压了。