ISET接的1K电阻,ISET2接地,按理应该输出500ma左右的的电流,可是给1200mah电池充电的过程中只有70ma,输出电压正常,4V。
还有连接CHG引脚的LED灯亮是表示充电完成么?
英语能力有限,从PDF上就看懂这么多。谢谢大家。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ISET设置充电电流,计算公式是KISET / RISET,KISET约等540,接1K电阻的话则ISET约等540mA。
ISET2设置Input/Output Current Limit,High = 500mAmax, Low = ISET, FLOAT = 100mA max,悬空说明输入最大只能100mA。
CHG灯亮说明正在充电。
你没的是输入电流还是电池端电流?
试下把电池电压放到4V以下比如3.8V再测下充电电流?