This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27441,锂电池老化后校准问题!



电池使用一段时间后,偶尔出现10%甚至更高剩余电量时就自动关机。关于该现象小弟一直有一个疑问:

锂电池出现老化后,电量计是如何重新校准电池计量的?电量计是否再使用过程中有一个自动学习的功能?

  • BQ27441采用的是阻抗跟踪的算法,这个算法在整个电池的使用过程中,会实时的测量电池的内阻变化进行电量的计算。电池老化之后,会体现在电池内阻增大,这个时候电量计也能够相应的计算得到。但是这个内阻的计算有个前提,那就是首先需要学习到电池的Qmax,而Qmax的学习需要在一次超过37%的充电过程或者放电过程的前后都有一次静置的过程,能够测量到OCV。这样子就能够自我学习了。