Other Parts Discussed in Thread: LM1117, LMR14020, TPS5405, TPS5402, TLV1117, TPS5403, TPS54260
你好!打算做一个电源小板子,电源输入12V,输出5V/500mA,较低纹波。
考虑到散热问题,12V转5V打算用DC/DC + LDO的方案,能否推荐一下适合该种方案的 DC/DC 和 LDO。谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
12V转5V采用DC-DC一级就可以解决效率和热的问题。 有非常多的选择。比如,其中TPS5405是一个5V固定输出的DC-DC,在工业家电等领域成熟应用多年,可以放心使用。
regards,
Patrick
Hi,
稍微补充一点,采用单个DC-DC如TPS5405,纹波也能够做到20~30mV,对于普通应用也足够了。如果要求非常高, 可以采用TPS5402+tlv1117.谢谢~
Regards,
Patrick
你好,TPS5402是固定输出的吧,手册里没有看到克调节输出啊。这样的话我转5V再接LDO输出就小于5V了,就达不到我的要求了。
您好,
TPS5402是可调的,通过外面分压电阻调。 TPS5403是固定3.3,5405是固定5.
regards,
Patrick
你好,TPS5402手册里貌似没有给出分压反馈的计算公式,那怎么调节呢?