This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

3000W大功率电源有什么方案可以解决

Other Parts Discussed in Thread: UCC28180, UCC28950, UCC25600, UCC28070

最近碰到一个难题,为超声波粉碎机制作一个大功率电源,功率为3000W,不知道各位大神有什么好的解决方案,提供参考下,谢谢

  • Hi,

      3000W大功率有很多拓扑结构可以选择,这里介绍两个比较高效和成熟的方案:

      1. PFC+移相全桥: UCC28180+UCC28950. 移相全桥对于3000W的应用,从效率EMI成本体积的角度都是非常非常合适的。

    2. PFC+ LLC: UCC28180+UCC25600. LLC是谐振式变化拓扑,可以进一步降低开关损耗和优化EMI,但是在3000W的应用中对谐振槽的参数优化要求更高,设计难度会大一些。

    谢谢~

    Regards,

    Patrick

  • 我这个3000W,电源主要作为大功率超声波细胞粉碎的驱动电源,这个在设计的时候,如果采用PFC+移相全桥有什么注意点没.,能不发一份相关PDF借鉴下,谢谢

  • 3000W的PFC要用UCC28070

  • Hi,

      我不清楚您的超声波细胞粉碎驱动电源有没有什么特别的要求,纹波小?效率高?或者其他的。TI有基于UCC28180的3.5KW方案,以及基于UCC28950移向全桥的方案,都可以在官网上下载到资料。 当然,如楼上所说,如果您想要有更小的体积和更好的纹波要求,可以考虑用两相交错并联的方案,用UCC28070。

    regards,

    Patrick