This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77910A GND引脚



由于电路板空间限制能否将三个GND引脚直接接地?

或者将三个引脚直接连接,并通过一个电阻接地?如果这样,原1K阻值是否需要改动?

  • Shaoyang,

       GND是逻辑电平的地,直接与VSS相连。具体参考下面链接7.10的说明:

    www.ti.com/.../sluu368.pdf

    Pins 23, 24 and 25 of the bq77910 must be tied to GND for normal operation of the device. In an application these might normally be tied directly to VSS, on the EVM they are individually pulled down for possible future use. Pin 30 should not be connected in normal operation. The EVM provided the R30 pattern for possible future use, this would be omitted for normal designs. Pins 2, 4, and 37 are not connected.