This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TLV1117-50发烫的情况

Other Parts Discussed in Thread: OPA355, TPS54060

电为蓄电池12V  给OPA355供电     单电源供电   直接就12V降到5V  传感器和调理电路都在野外,最近正好比较热,而且是连续工作,

7V的压降是不是大了点?  还是因为最近天气热的原因,综合因素?

 我这样的应用情况是不是有必要使用DC电源芯片,OPA355可以正负2.5V供电,我想如果能使用一个DC降压芯片实现双轨输出 +-5V  然后接两个2.5V的 LDO  ,这样的方案是不是保险点? 

整个板子温度太高 我怕影响运放的性能  麻烦解答 谢谢