如果一个电池包电压最大电压是29.4V,最大负载电流是20A,容量是62.4Ah。根据slua760,与电流、容量相关的参数缩小1/3就可以了。即使把的Design energe scale设置为10,Design Energy仍然超过32767,这个参数如何设置呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果一个电池包电压最大电压是29.4V,最大负载电流是20A,容量是62.4Ah。根据slua760,与电流、容量相关的参数缩小1/3就可以了。即使把的Design energe scale设置为10,Design Energy仍然超过32767,这个参数如何设置呢?
可以尝试将Cells number 改成1, 等效为1节电池, 校准电压时 也通过scale的方式。
例如实际输入42V,10节电池,校准电压为4.2V, number series改为1.
这样也可以。