UCC3895正常工作的时候是改变EAP脚的电压来进行移相,那我请问一下,如果EAP的电压为0会不会在移相?会产生什么情况?如果EAP为3.6V又会不会移相?又会产生什么情况?正常工作的时候EAP脚电压的变化范围让它变化多少?是2V-3V之间变化?还是怎么变化?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
UCC3895正常工作的时候是改变EAP脚的电压来进行移相,那我请问一下,如果EAP的电压为0会不会在移相?会产生什么情况?如果EAP为3.6V又会不会移相?又会产生什么情况?正常工作的时候EAP脚电压的变化范围让它变化多少?是2V-3V之间变化?还是怎么变化?
Hi SU JIANFEI:
首先需要知道,UCC3895移相控制主要是依靠C和D与A和B的相位移动产生的,A和B的相位是预先由芯片确定好了的,两者刚好完全反相。至于稳态工作中的相位移动多少是由占空比决定的(不考虑占空比丢失), 也可以说是由负载条件决定的, 同时也可以说是由反馈脚电压决定的,正如你所说的那样,它取决于EAP或COMP脚电压。如下所示:

如果你对3895构架感兴趣,完全可以将EAP脚电压与输出负载条件用一个函数关系式表示出来,甚至可以将EAP脚电压与移相大小表示出来,随然花时间,但如果是你亲自完成该项工作,相信你将在以后的UCC3895的设计和调试中会非常有经验。
好吧,现回答一下你的问题:
1.如果EAP的电压为0会不会在移相?
首先EAP在稳态中是不可能为0的,清载条件下为了达到一个最小的占空比,反馈脚电压肯定是要和内部的斜坡作比较,UCC3895的最低斜坡电压是0.8.所以EAP的最低电压应该要高于0.8。
2。EAP的电压为0会产生什么情况?
不工作。
3.如果EAP为3.6V又会不会移相?
一般来说,会移相,只要电源能稳定工作。移相大小取决与斜坡补偿的设定和负载条件,如下图。反正一定负载条件下PWM COMPARATOR 的输出占空比是大致既定的。
4.正常工作的时候EAP脚电压的变化范围让它变化多少?
取决与斜坡补偿的设定和负载条件,也可能是在2V-3V之间,也可能在1-3V之间。
最后来一张UCC3895的内部原理图,你可以仔细研究研究TI的移相全桥霸主.

Su Jianfei Su :
请下载以上UC3895 MODEL.pdf.
如果你很精通UC384X内部逻辑原理的话,看这个还对你理解UC3895有点帮助.不然将会很耽误您的时间的.毕竟你们是侧重于电源应用和设计的.
Have create classic Pulse Width Modulation (PWM) with UCC3895. In this patent create PWM and phase shift. http://www.google.com/patents/US20090196072