This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps2419芯片电压从C输入,那么A脚会不会有电压输出

Other Parts Discussed in Thread: TPS2419tps2419芯片电压从C输入,那么A脚会不会有电压输出,因为我想在A脚并联一个发光二极管,当A脚也就是NMOS的s极有电池接入二极管就亮,无电池接入就不亮。
  • 您好,

      从C输入,A是不会有电压输出的,至于后半段的描述我没有太明白您的意思。

      谢谢~

    Regards,

    Patrick

  •  就是我想用TPS2419控制NMOS将蓄电池接入供电电路中,然后在蓄电池这一侧接个发光二极管串电阻到地,如果有蓄电池发光二极管会亮反之熄灭。但是实际情况是,当没有蓄电池时,发光二极管也会亮,也就是说,芯片C端连接着我的供电电路,当没有蓄电池时,我的供电电路的电压会从芯片C端进入,然后A端会有一定的电压输出,足以点亮发光二极管。不知道这样说明您有没有看明白。

  • 就是我想用TPS2419控制NMOS将蓄电池接入供电电路中,然后在蓄电池这一侧接个发光二极管串电阻到地,如果有蓄电池发光二极管会亮反之熄灭。但是实际情况是,当没有蓄电池时,发光二极管也会亮,也就是说,芯片C端连接着我的供电电路,当没有蓄电池时,我的供电电路的电压会从芯片C端进入,然后A端会有一定的电压输出,足以点亮发光二极管。不知道这样说明您有没有看明白。

  • 你C端电压多少?现在A端电压多少?

  • C端电压13.8V,A端不接除MOS管以外的东西是11V左右,接了发光二极管串7.5K电阻会有6V多电压