This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76920 关于测量电压读数的问题



接通电路之后,发现从VC1到VC5都没有电压数据,这是为什么呢? 查看SYS_CTRL1的值是16,(也就是说只有ADC是启动的)SYS_STAT的值时2。我要测量的是3节锂电池串联的电池组(工作电压为11.1V),所以我把V2,V3,V4引脚短路在一起。我的控制器是TM4C123G的开发板。我用电压表测量了一下VC0到VC5各个引脚对地的电压,分别是6.32V 5.60V 4.76V 4.76V 4.76V 3.95V(电压这么低是因为pin脚到电池平衡器端口之间接入的电阻有关?) 没有值是因为电池处于SHIP状态吗?

如何判断芯片是否处于SHIP状态呢?

还有一个问题就是,VC5一定要接电池电压最大的一端,VC1接电池电压最低的一端吗? 可以让VC5接电压最低端,VC0接电压最高端吗?

求大神解答!