项目要做一个电池充放电,给4节串联的3000MAH的18650锂电池充电,管理芯片要带充电平衡功能,不要带IIC口的,要求封装是SOP类的,只要模拟电路的,不要带单片机的,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
项目要做一个电池充放电,给4节串联的3000MAH的18650锂电池充电,管理芯片要带充电平衡功能,不要带IIC口的,要求封装是SOP类的,只要模拟电路的,不要带单片机的,
希望有平衡功能,不然不放心电池,对这个不是很了解,不知道不平衡带来的伤害,所以还是带平衡好点吧,UCC3957怎么样,我跟别人说这个片子,别人一脸惊讶,问我为什么用这个片子,UCC3957不好么? 期望片子最好有demo的文档,看看各种参数,了解了解情况,学习学习,做起来心里更有底, 还有芯片工作温度要宽一点,零下20度到70度+, 看了下BQ77905,感觉还不错, 觉得BQ77905和UCC3975差不多, 但是BQ77905因为温度保护做的比较好,可能达不到我要求的宽工作温度,
UCC3957是controller 芯片。 不是BMS管理的, 温度保护可以不用,或者接一个固定电阻就好。
demo和datasheet 在ti官网都可以搜到;