This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24075充电问题

Other Parts Discussed in Thread: BQ24075, BQ24075T

我最近负责的一个项目用到了锂电池充电模块,采用了BQ24075作为电源充电管理芯片,其原理图如下所示,但是工作异常,表现为充电指示灯亮,但是实际没有冲进去电。

目前电路实际情况为:

1. 电池电压3V,当一直有外部电压供电的时候,还是一直是3V,冲不进去电;

2. TS端下拉了一个10K的电阻,量两端电压,为零,表明电路工作异常;

3. ILIM以及ISET电阻两端电压也为零;

4. CHG以及PGOOD电源指示灯全部亮,表示外部电源供电正常并且充电正在进行;

但是问题在于,我冲了几乎一整天,电池电压还是3V,请TI的专家帮忙看一下我的电路,是否存在一些我们使用上面的问题,谢谢!