经过社区上各位大神的解答,现在已经可以通过控制器(TM4C123G)与BQ76920进行通信了,并且可以正常读出各个寄存器里的数据。但是新的问题是,我尝试写入新的值到控制寄存器(例如 SYS_CTRL2),以激活库伦计(CC_EN)。但是写不进去,写完再读取寄存器的状态,显示还是原来的值。这是为什么呢?
附上我的写入代码,望各位大神斧正
比如我要是想写入0100 0000的话,在指令里直接写入64就可以了吧? 如 I2CSend(0x08,2,0x05,64)
void I2CSend(uint8_t slave_addr, uint8_t num_of_args, ...)
{
// Tell the master module what address it will place on the bus when
// communicating with the slave.
I2CMasterSlaveAddrSet(I2C0_BASE, slave_addr, false);
//stores list of variable number of arguments
va_list vargs;
//specifies the va_list to "open" and the last fixed argument
//so vargs knows where to start looking
va_start(vargs, num_of_args);
//put data to be sent into FIFO
I2CMasterDataPut(I2C0_BASE, va_arg(vargs, uint8_t));
//if there is only one argument, we only need to use the
//single send I2C function
if(num_of_args == 1)
{
//Initiate send of data from the MCU
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);
// Wait until MCU is done transferring.
while(I2CMasterBusy(I2C0_BASE));
//"close" variable argument list
va_end(vargs);
}
//otherwise, we start transmission of multiple bytes on the
//I2C bus
else
{
//Initiate send of data from the MCU
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_START);
// Wait until MCU is done transferring.
while(I2CMasterBusy(I2C0_BASE));
//send num_of_args-2 pieces of data, using the
//BURST_SEND_CONT command of the I2C module
int i =1;
for( i = 1; i < (num_of_args - 1); i++)
{
//put next piece of data into I2C FIFO
I2CMasterDataPut(I2C0_BASE, va_arg(vargs, uint8_t));
//send next data that was just placed into FIFO
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_CONT);
// Wait until MCU is done transferring.
while(I2CMasterBusy(I2C0_BASE));
}
//put last piece of data into I2C FIFO
I2CMasterDataPut(I2C0_BASE, va_arg(vargs, uint8_t));
//send next data that was just placed into FIFO
I2CMasterControl(I2C0_BASE, I2C_MASTER_CMD_BURST_SEND_FINISH);
// Wait until MCU is done transferring.
while(I2CMasterBusy(I2C0_BASE));
//"close" variable args list
va_end(vargs);
}
}