This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教TPS62000输出不正常的问题

Other Parts Discussed in Thread: TPS62000

最近使用TPS62000做5V到3.3V的电压转换,电路如图所示。遇到比较奇怪的问题:

1、电路板焊好后,测量3.3V输出,只有2点几伏,测量FB脚电压0.45V。

2、怀疑电路出现虚焊,用烙铁点了一下TPS62000的各个引脚,重新上电测量,电压输出为3.35V,FB引脚为0.45V,电路似乎正常了。

3、奇怪的问题出现了,电路在断电超过2小时后,重新加电,输出又不正常了只有2点几伏,重复过程2,烙铁点一下,又恢复正常。

可以确认的是电路没有虚焊,仔细检查过,而且上述过程重复了4、5次,现象是相同的,每次只要长时间断电,重新加电肯定是输出不正常的。似乎是烙铁加热一下就恢复正常,而且在一两小时内反复测量是没问题的。

  • 1. 能将EN脚跷起然后串联一个10K电阻到VIN,让EN Delay一下试试么?!

    2. 你所用的陶瓷电容是否有Y5V的?若有,都换为X5R或X7R的试试

    3. 芯片的供货渠道是否OK?

    从你的线路图来看到没什么大问题!