Other Parts Discussed in Thread: BQ51013B, BQ51010B, BQ51221, BQ500215, BQ51025
TI各位大哥,跟你们询问下,BQ51013B是不是出了升级版本。型号是什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不存在升级,只是你的应用产品的定位是什么功率等级和应用场景。根据应用选择合适的方案。
BQ51013B是早期针对低功率等级<5W,由于散热问题,实际做到3.5W左右,更适合小功率设备。后续出的是BQ51010B,输出电压7V,这样相同功率,输出电流减小,可以提供更好的散热,输出功率做到5W左右,可以认为是BQ51013B的改良版本。
之后的BQ51221是支持双模5W模式,因为PMA和A4WP联盟合并,市场上基本是WPC和PMA的协议方案。
BQ51025支持接收端10W的方案(但是必须和BQ500215搭配才能输出10W),是和发射端和接收端都做的厂商。
谢谢。