Other Parts Discussed in Thread: BQ25101, TPS62743, BQ25101H
Ti专家好:
以上是我的一个120mAh的锂电池应用,目前出现这种情况:
使用中发现如果接上,在没有电池的情况下,插入usbbq2510不工作,输出在1.96v左右,并且这种情况偶尔会消失.另外在没有外部usb电源输入的情况下,如果电池电量消耗到0时,插入usb电源很多时候并不能让bq25101输出4v左右供电池充电,同理后面的tps62743同样也因为输入电压不够导致不能给后面的电路工作.
请问1,这种现象正常吗,电路或者使用上有什么不妥当的地方吗?
2,电路还有什么需要注意的吗?
3,请指导下这种电路的充满电后可以使用的时间(如果vcc和vccA后面都没有负载)