Other Parts Discussed in Thread: TPS562201, BQ24196, TPS54331
所需参数:
电压输入为 12V.也可降压.
电流输入为 1A.
但电流输入不稳定,有波动.
输出电压 5V
输出电流 500mA-1A均可以.
主要是给手机充电用.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
性价比高的,TPS56220x这些都可以。
http://www.ti.com/lit/ds/symlink/tps562201.pdf
谢谢。
TPS54331一类的降压都行,给手机充电不需要恒流芯片,只需要恒压限流芯片。如果是给电池充电,那么需要BQ24196一类的充电管理芯片。