我想做+60和-60V稳压电路,目前已知TL783可以做+60V,请问有没有和它相对应的负电压稳压芯片,要求指标参数和TL783一致,就比如LM317和LM337
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
一般高压的LDO通常是针对输出电流比较小得应用,例如100V的TPS7A4001,最大输出电流50mA。原因是电流一大,很容易造成非常高功耗,散热很难做。而且效率非常低。
一般这种情况会先用DC/DC,如果你对输出纹波noise要求很高,可以再高低压转换成为低电压后再增加一级LDO.
您好,
TI没有-60V的LDO, 可以考虑用DC-DC的结构实现稳压电路,谢谢
Regards,
Patrick
Hi
没有-60V的LDO.
如上建议,增加一级负电压转负电压的DC/DC.
Hi
你的输入电压是多少? 是否有选择?
60V/-60V输出负载是多少?
我看一下是否有合适的方案推荐。