This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3481有两个问题请教



问题1:我想设计5.5V启动工作,5V欠压保护,根据官方计算问题如下:

最后试验结果是:5V可以达到欠压,但5.5V无法开机,最后输入电压到9V左右才能开机,哪里计算错了呢?

问题2:我把R7=100K,R8=75K,目的是从4V左右就开始工作,然后我把直流源调到6V,电流放到最大,输入接了220uF电解电容,我想测测带载开机等电性能,发现空载、半载5W可以起机,输出电压正常,但是带满载10W就无法开机了,无输出,芯片驱动会发出连续10几个脉冲就关了,问题可能是出现在哪里呢,图纸是按照附件画的正式PCB。

附件文档有个测试条文:空载开机,等输出建立再投载,这难道是暗示不能带载起机?

snvu528.pdf