This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ3060 Max Error始终是8%

Other Parts Discussed in Thread: BQ3060

BQ3060的CEDV配为00,EDV0 EDV1和EDV2的参数是正确的(学习出来的FCC值也是对的),Battery Low%=EDV2=7%或者18%我都试了,,但Max Error始终不对,一直是8%,我查过相关资料,8%是有限制的学习,因此我就搞不明白了,到底是哪个参数设置不对,限制了它,我想请教一下,这个Max Error除了与EDV0 EDV1和EDV2相关之外还跟哪些参数值相关,该样设置?用的是3串两并的电芯,总容量是4300mAh,下面是我认为对Max Error有影响的参数值及设置值

CEDV=00

EDV0 EDV1 EDV2确定正确

DesignCapacity=4300

DesignVoltage=11100

RemainingCapacity=430

QMax1 2 3 4=4300

CC% Thresholds=3870