This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问BQ24745给NiMH和NiCd电池充电,如何设置?

Other Parts Discussed in Thread: BQ24745

请问BQ24745给NiMH和NiCd电池充电,如何设置?

1、在BQ24745里有提到

Charge Any Battery Chemistry: Li+, NiCd,
NiMH, Lead Acid, Etc.

但是不知道如何进行设置。

Simplified SMBus Control Interface system power-management microcontroller using the
– Charge Voltage DAC (1.024 V–19.2 V) SMBus interface. 
– Charge Current DAC (128 mA–8.064 A) 5-mm × 5 mm QFN package.
– Adapter Current Limit DPM DAC (256
mA–11.008 A)

而SMBus只是设置充电电压、电流,和适配器的限制电流。