Other Parts Discussed in Thread: TPS43061
各位大神好! 本人用TPS43061做了一个 输入DC10~18V,输出DC 25.4V/4A 的方案,现在问题是下管温升严重,达到110摄氏度,请问是否我的参数有问题,还是本身这方案不能做到这样的功率,附件原理图
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TPS43061
各位大神好! 本人用TPS43061做了一个 输入DC10~18V,输出DC 25.4V/4A 的方案,现在问题是下管温升严重,达到110摄氏度,请问是否我的参数有问题,还是本身这方案不能做到这样的功率,附件原理图
你好,
你FET的导通阻抗多大的,驱动电阻也选小点,先上0ohm看看。
Chelsea :
谢谢你及时回复,我选择的MOSFET都导通阻抗是3mOhm的,但是我用WEBENCH模拟典型电路及模拟温升同样是非常高的,这是什么问题,是否是需要额外增加散热处理?附件是我导出来的报告。驱动电阻在测试过程时也改为0了
你好,
那估计本身损耗就会使电路有这么高的温升,所以你可以选更小热阻的MOS(跟封装有关系),或者加大板上的铜厚
Chelsea
你好,请问在BOOST电路中,下管是否都是比上管热的,在相同MOSFET情况下,如果下管并联多一个MOSFET是否会有帮忙,谢谢!
你好,
你要看你的占空比,比如输出电压高,下管导通时间长,下管导通损耗会稍稍大些。
并联MOSFET肯定有用,另布线时尽量保证驱动线差不多。