This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40304输出电压低,无法带载

Other Parts Discussed in Thread: TPS40304

设计指标
输入电压5.5-12vdc,输出电压2.4v,电流12A
原理图按照TPS40304规格书13页,8.2.1 Figure 14.(在此图上基础上修改)
输出分压电阻R4改为15k,输入输出电容增加,L1电感量0.46uH,mos管都使用CSD16322

问题是:输出达不到设计电压(只有1.6v),根本无法带载,很小的负载就保护使输出电压为零
检查后发现2脚(en)电压是锯齿波形,(  VBP为6.5v正常,两个mos的栅极有间隙工作的驱动电压约5v,sw脚也正常连接了)
如果2脚(en)直接接地,那输出电压为零
如果2脚(en)接上拉电阻200k,输出只有1.6v,波形为三角波

就不知道怎么处理这个EN脚了???

另外,pgood是输出电源好功能脚吧?也以上现象无关吧?