This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq78412使用问题

Other Parts Discussed in Thread: BQ78412

想请教一下高手们,小弟最近在研究bq78412的EVM,碰到了很多问题,希望同仁们给予一下技术支持,多谢

1、在78412自带的那个软件里面在配置默认参数时需要存储一个CSV文件,当对铅酸蓄电池进行一轮化学参数学习后,该铅酸蓄电池的化学参数是否也会默认存入CSV文件;

2、该芯片有对寿命预测的一些算法,能否通过一些命令调出SOH计算的内部参数表格;

3、TI是否有针对2节或多节铅酸蓄电池串联的寿命以及电量预测芯片;

4、自带软件中的chem ID的内容主要是内阻、温度以及一些老化参数。请问这里提到的老化参数有哪些具体参数?

5、芯片检测到的内阻、温度、电压、电流、老化参数等参数,通过通信外部CPU是否可以读取到?

6、SOH的计算是通过采集外部的一些参数来和78412内部的一个数据表进行对比得出寿命预测,那个数据表里面主要有哪些参数,在进行寿命估测时,是优先匹配内阻?温度还是其他参数?或者有一个优先级?能否给予详细解释

7、datasheet中提到这个learning的过程是从放光再充满,想问一下learning过程必须要严格的放光才可以么?在learning过程前需要设置哪些参数?

8、我们的使用环境描述:在出厂之前,我们可以可以进行蓄电池深度放电learning。但在运行现场只能进行浅度放电,如果只能进行浅放电,是否会影响测量结果以及寿命的预测?

9、每次learning之后,所学得的关于铅酸蓄电池的一些例如容量的参数能否通过一些命令或那个软件调出?

10、考虑到铅酸蓄电池是不允许进行过充和过放的,我们如何实现learning过程?

11、我们通过Demo板测到蓄电池的SOCSOH,请问您有没有方法推荐给我们来验证这些参数的可靠性和精度?

12、P-Scale什么意思?

13、MeanscaleRS+RS-间的电阻值)无法写入

14、放电时,LED显示时间是否通过DsplyConf1来设置,但是没找到设置入口;充电时,LED显示是基于capacity in amp-hoursDevConfig1[5:2]LED显示个数来确定的,何为capacity in amp-hours