Bq51050B支持5W的充电功率,Pin12 ILIM脚设定充电电流的大小500~1500mA,
假设给标称4.2V锂电池充电时,如果充电电流设置为1A,那么充电过程中,电流上升到1A后即保持恒流充电,充电电压将从一个较低的值逐渐上升并接近4v,在这个过程中,充电电流保持恒流1A充电,也就是说充电功率逐渐达到4W,那么我有下面几个问题如下:
1.此时无线发送器线圈和接收器线圈的功率有多大?
2.接收器线圈的电压和电流是不是分别是4V和1A?
3.发送器线圈和接收器线圈电压是相等呢还是等于线圈匝数比?
4.发送器线圈输出功率传递给接收线圈时,损耗有多大?