Other Parts Discussed in Thread: TL494
根据TL494的规格书,最高规格要求为-40℃-85℃。现采用该芯片的电源环境使用温度为-40℃-75℃,高端温度无法满足要求。TL494实际高温能到多少度?如不能满足要求有相应替换芯片吗?(直接替换)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TL494
根据TL494的规格书,最高规格要求为-40℃-85℃。现采用该芯片的电源环境使用温度为-40℃-75℃,高端温度无法满足要求。TL494实际高温能到多少度?如不能满足要求有相应替换芯片吗?(直接替换)
85C指的是使用时最高的环境工作温度~
请问实际工作时确实会发生过温的情况么?
TL494ID的最高工作温度是85度。
这里的85度指的是在无风扇散热条件下的工作的环境温度,所以如上所述的工作条件是没有问题的。
经实际测试,电源置于环境温度80℃环境温度,494芯片表面温度远高于85℃仍能正常工作!