This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS74401上电顺序是否会导致输出异常?

Other Parts Discussed in Thread: TPS74401

我使用TPS74401给FPGA的高速收发器供电,估计电流约为300mA。供电时两种供电方式二选一,EN与IN直连。

第一种供电是12V产生3.3V和5V电,分别作为VIN和BIAS,这种情况电路工作正常。(此时3.3V和5V几乎同时上电)

第二种是使用5V产生3.3V作为VIN,同时5V作为BIAS,此时3.3V滞后5V约8ms,这种情况芯片工作大约两分钟就无电压输出了。

看手册里面我这种属于典型用法。两种使用方法的主要区别是供电时序,但这种现象手册里没有说明。

请问这种情况有没有解决的措施或解释?

谢谢