1、接上D1 D2有什么好处?如果去掉有什么影响吗?还请TI专家帮忙深入解释下。
2、为了简化电路,Q1 Q2可以只保留Q2吗?这样做会多出什么不安全隐患吗?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. D1, D2是用来选择供电电源的,D1表示由输入适配器给芯片VCC供电,D2表示由电池给芯片VCC供电。都去掉,就无法供电了。
2. Q1是启动过程中,缓冲开通,使得适配器电压和电池电压不会瞬间短路。假设没Q1,在适配器插入前,system由VBAT供电,此时插入适配器,将发生适配器和电池电压瞬间短路,造成瞬间充放电。造成适配瞬间过载,也会在Q3上产生瞬间大电流,可能损坏Q3
D2去掉的话,在不插适配器,仅有电池的情况下,芯片没有供电。这样,如果system需要供电,电池供电回路battery->Q3->system,由于芯片没有供电,Q3的驱动不会打开,电流只能经过Q3的体二极管(压降1V左右),在其上的损耗比较大。
不是。芯片不供电的时候,Q3肯定是关断的。重新检查你的测试。