我需要一款输入电压14~18V,可以输出5V 12V的固定或可调稳压芯片,要求输出电流300mA以上,给数字电路和模拟电路供电,纹波尽量小。TI电源芯片太多,还请有经验的工程师推荐几个合适的型号,谢谢了!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
还是建议你用DC/DC, 你算算如果是18V输入,5V输出,压降就有13V了,将近4W的损耗,一般LDO受不了的。
对于5V输出的,建议用DCDC加LDO的方式吧。
先用DCDC把电压降到5V以上,然后在选一个low ripple的LDO
Hi,
如果您是需要5V输出,300mA以上,考虑压差太大发热太严重,建议采用DCDC方案
Regards,
Patrick