我目前使用TPS767D301来作为3.3V以及1.9V电压输入是5v,目前芯片发热严重,室温下都有70度,
能否推荐下最新的dc-dc芯片,
5v输入,3.3v输出,1A;5v输入,1.9v输出,1A左右的芯片.
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
LDO效率本身比较低(Vo/Vin),功耗也会比较大[(Vin-Vo)*Io], 按照你上述的功耗,都接近5W了,就算热阻是20℃/W 温升都接近100℃了。
Hi
从你50℃的温升看,实际电流是小于1A的,70℃不算很高没有问题。
一般100℃以内都可以接受,如果环境温度较小无法兼顾就选择DC/DC.
请问使用TPS62240是要调整到1.9V输出吗?还是用默认的1.8V就可以?