This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27441的Taper Rate参数应该是多少

Other Parts Discussed in Thread: BQ24079, BQ27441-G1

我用bq24079作为充电控制芯片,用bq27441做电量计。

对于bq24079,如果充电时系统断开,不给系统供电。

当EN1EN2=01时,限流由外部电阻决定,我取的RISET=820欧姆,所以ICHG = KISET/RISET=1085mA

当EN1EN2=10时,限流500mA,所以ICHG = 500mA

因此

参照bq27441_quick_start.pdf,Iterm按上限取。所以Iterm=0.11*Ichg

Taper Rate = Design Capacity / (0.1 * Taper Current)

我的电池为2000mAH,所以我计算Taper Rate:

 

EN1EN2=01

EN1EN2=10

ICHG

1085mA

500mA

Iterm

119mA

55mA

Taper Rate

168.1

363.6

应该没有算错吧。

但是bq27441-G1_TR.pdf上却写:

单位是0.1Hr,所以Taper Rate最大值是200。

Q1:那么bq24079的EN1EN2=10时,计算出的Taper Rate=363,超过了200,应该怎么办?

Q2:在上述计算时Taper Current是按照CHG Current的比例计算的,是在系统不加电的情况下计算的。如果充电时系统也在工作,一部分电流被用来给系统供电,那么由于限流的限制,实际的CHG Current就减少了,并且随系统工作状态变化而变化。在这种情况下,Taper Current还照原来那样计算吗?会造成电量监测不准吗?

Frank