This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

电源模块IC



有没有关于实现+12V或者+24V输入,-15V~+15V范围的可调电压输出功能的电源管理芯片推荐?

  • Hi,

      任何选型都是需要参数条件,请问确定需要的输入电压输出电流,是否隔离,以及其他要求等,谢谢

    Regards,

    Patrick

  • 其实我想做一个大概的数字电源:从一个大概12V或者24V的适配器接入,当做输入电压,经过变压芯片得到-15V至+15V范围内可调的电压。输出电流不能过大,没有特别的具体要求,隔离电源。主要给薄膜晶体管供电,给芯片供电即可。希望能推荐一些可供选择变压的芯片,谢谢!