Other Parts Discussed in Thread: TPS54340, LM22670, TPS54060, TPS54040, TPS62130A
您好,
TPS54340规格书上看到正负压的电路拓扑结构上标明这颗IC理论上是可以输出负压的,请问该芯片能实现+5V到-5V的输出么?能否简单说明一下,多谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
TPS54060的负电压输出文档: http://www.ti.com.cn/cn/lit/an/slva317b/slva317b.pdf
这两个芯片是非常接近的,TPS54060是TPS54040的60V版本输入,TPS54340是TPS54040的3.5A版本输出。
Hi
如果是5V转-5V, 电流1.5A以内,或者你还可以选择同步芯片TPS62130A:
http://www.ti.com.cn/cn/lit/an/slva469c/slva469c.pdf
注意一旦设计成为负电压输出,最大输出电流不在是原来正电压输出的规格,是要打折扣的。