This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ucc28070如何单板调试

Other Parts Discussed in Thread: UCC28070

请教大神,在使用TI的300W交错并联PFC的方案时,设计到ucc28070,最为主电路的控制芯片,只有确保了其输出的正确性才能与主电路连接,请问:

如何在不与主板连接的条件下如何对ucc28070进行单板调试,请大神指导

  • 亲;建议用低压做个工装,测量调试。

  •  

    您好:请问你的意思是说

    1、用VSENSE、Vinac、CSA、CSB这几个端口作为输入端吗?

    2、可以将VCC的输入电压分压成3V送给这四个信号,可以吗?分压电阻选成千欧级的,可以吗?

    3、如果是单板调试,是不是只涉及到这四个输入信号呢?(VCC\GND),还有其他的吗?

    请指教,麻烦了,谢谢。