This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq30z55 怎么做补偿容量



各位大神,目前我这个3S项目,因为客户设备加的外设比较多,功率一定,当电池电压降低的时候,过的电流会增加。

当外设全部加上的时候,测试出来当电池电量在15%(大概10.4V左右)的时候电池会保护,而设备没有启动关机流程,

我想将此电压(9V到10.4V)做0%电量点或者10.4V做0%电量点,这样当设备用到0%(10.4V)的时候启动关机流程,而电池不会保护。

这样我该怎么设置???

比如将电池关机电压从原来的3.0V设置为3.45V即可,再做次学习?

还是其它参数也需要更改???