输出电流设置为620mA,R1为10K,R7、R8为1K,R9为0.2。当IS管脚接到Q1漏极,R6短路时,实际输出只有50mA,R9两端电压与安照Datasheet里公式计算出来的结果差很大。当IS管脚按图中方式接Q1源极,R6为0.05时,输出电流为700mA,但Q1发烫严重,总的输入电流有2.5A左右。总的输入电压为7V。这是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
输出电流设置为620mA,R1为10K,R7、R8为1K,R9为0.2。当IS管脚接到Q1漏极,R6短路时,实际输出只有50mA,R9两端电压与安照Datasheet里公式计算出来的结果差很大。当IS管脚按图中方式接Q1源极,R6为0.05时,输出电流为700mA,但Q1发烫严重,总的输入电流有2.5A左右。总的输入电压为7V。这是什么原因?
升压电路,输入电流的大小与输入、输出电压相关。如果输出电压比较高,输入电流会比较大。
如果MOS管没有散热器的话,温升确实会比较高。
建议可以考虑CSD19xxx系列QFN封装,通过PCB来散热。
应该不是MOS管的问题,之前的频率设定为250KHZ,现在改为600KHZ效果好了点,MOS管不烫了,但电流与理论计算还是差了200mA,现在实际电流是820mA。另外这个频率有没有要求?