This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请推荐一款+5V转-3.3V电源芯片,负载电流1.5A,纹波低于30mV.
可以看一下我们的LMZ34002。或自己用TPS62130,用以下的方式来实现。
Using the TPS6215x in an Inverting Buck-Boost Topology.. (Rev. C) (slva469c.pdf)http://www.ti.com/litv/pdf/slva469c
XL4003可以5V转3.3V,驱动能力强,可以输出4A电流。纹波30mV