This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于充电管理芯片BQ24610使用碰到的问题,请教。

Other Parts Discussed in Thread: BQ24610

我设计的充电电路输入电压额定为直流24V,充电电压输出额定为14V,在调试电路中碰到如下问题:

在充电电路空载(不连接电池组及其它任何负载)情况下输入直流18V电压,充电电路输出电压用万用表测量为13.92V左右,PG-LED点亮,其它两个LED不亮;用示波器测量输出电压波形,发现稳定值为14V左右,间隔大约530毫秒有峰值为5V左右的负边脉冲,如下图:

我将输入直流电压调整到24V,充电电路输出电压用万用表测量为12.8V左右,PG-LED点亮,STAT1-LED闪烁;用示波器测量输出电压波形,发现稳定值为14V左右,但是间隔大约1.2秒输出电压有明显的电压下降,充电电路工况一样,我只是调整了输入电压幅值,输出为何会有如此明显变化,如下图: