最近在给客户开发一个电路板,由于板子尺寸很小,所以选择一款24v转5v的LDO芯片,LDO芯片主要就带了一个AVr的单片机和3个led灯。我想咨询一下,这块芯片的发热量是多大。我是传感器使用,发热量太大会影响测试。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LDO的损耗跟芯片无关,等于(VIN-VOUT)*Iout。不知道你的IOUT就没法计算热量。知道了损耗之后,用损耗*热阻(环境-case)可以得到大概的发热。
Hi
功耗是(24-5)*50=950mW, DBV封装的热阻是212℃/W, 那么温升200℃左右。
DRV封装热阻是73.1℃/W,温升是70℃左右。
Hi
LDO应用上一般是压差比较低的时候或者电流非常小的时候,避免功耗比较大,造成温升过高。